Hard disk drives are today's fastest permanent storage media and have a large capacity. For this two reasons they are the most used storage medium in computers and servers. When buying a new hard disk, there are three important things to consider: - The connection of the disk to the computer or other device you will be using it with has a big influence on the speed with which data can be read from/written to the disk. Make sure the connection of the disk you buy is compatible with your computer! - The rotational speed is also important for the speed with which data can be read from/written to the disk and determines the time it takes to find a file on the disk. - Last but not least, the storage capacity of the disk, i.e. the amount of data that can be stored on the disk.
A 500GB Serial ATA 3Gb-per-second Apple Hard Drive operating at 7,200 revolutions per minute. Works with Mac Pro.
Mac Pro supports up to four 3Gb/s Serial ATA hard drives for up to 2TB of storage. The new cable-free, direct-attach drive solution lets you install and remove drives in a snap. To install a drive, you connect a simple drive carrier to the hard drive, then just slide it into place
...
More>>>
— no cables or connectors to hassle with. Removing the drive is just as easy. Every Mac Pro ships with four hard drive carriers. This solution is perfect if you ever share drives among different workstations at home or the studio.
<<<Less
Specs
Alternatives
Options
Disk drive
Internal
The device is built in, or needs to be built in (Yes/No). No, means that the device is connected externally via wire or wireless.
Hard disk rotational speed
The rotational speed of a hard disk expressed in rotations per minute. The faster the better.
7200 RPM
Disk drive
Hard disk drive capacity
The maximum storage capacity of the hard disk in gigabyte (1 GB = 1 billion bytes).